8/21/2017 8:21 AM | |
Posts: 1 Rating: (0) |
Can I find "cross-cutter" code for s7-1500? If not, is there a posibility to get through with migration? Is it better to try writting code from the beggining or migration option in TIA could handle it? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/21/2017 8:32:12 AMNew subject after splitting |
|
8/21/2017 9:07 AM | |
Joined: 10/11/2006 Last visit: 10/14/2024 Posts: 5913 Rating: (809)
|
Hello, there is a cross cutter application for SINAMICS S120 (calculated in DCC directly inside the drive). Additionally there is a function block (LMCSINA library) for SIMATIC S7-1x00 to control this drive functionality from your PLC side. Here the link to the application: https://support.industry.siemens.com/cs/de/en/view/109477746 If you don't have a SINAMICS S120 available, you will need a SIMOTION controller or I guess a S7-1500T to calculate the cams. For SIMOTION there is also an application available. For S7-1500T up to now there is no ready-to-use application, but I guess in the future there will be released one. |
With best regards, |
|
10/18/2018 9:39 PM | |
Joined: 1/20/2010 Last visit: 8/3/2021 Posts: 5 Rating: (0) |
Hello, Did anything change? Is there now an application of flying sow for plc 15xxT?
|
10/19/2018 7:15 AM | |
Joined: 10/11/2006 Last visit: 10/14/2024 Posts: 5913 Rating: (809)
|
Hello, yes, there is an application available now: https://support.industry.siemens.com/cs/ww/de/view/109757260 |
With best regards, |
|
10/29/2018 12:27 AM | |
Joined: 1/20/2010 Last visit: 8/3/2021 Posts: 5 Rating: (0) |
Thank you, but is there an application for flying saw for PLC15xxT?
|
10/29/2018 1:16 PM | |
Joined: 5/6/2010 Last visit: 10/14/2024 Posts: 1984 Rating: (278) |
Hello bozzec, here is the link to the flying saw with a S71500T. regards |
Last edited by: Jen_Moderator at: 10/30/2018 7:32:07 AMOptimized link. |
|
Follow us on