3/27/2019 9:57 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
In network project is program language only FBD. |
3/27/2019 10:05 AM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
Take a look at attachment, it's a page of the manual.
AttachmentLOGO! 8 Soft Comfort Online-help 2014_06 page 368.pdf (364 Downloads) |
3/27/2019 10:56 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
If you want to create ladder programs, then you have to define the network settings manually and you get for each Logo an own program file. See this thread for example. Regards, Scorp |
3/23/2020 7:44 PM | |
Joined: 12/18/2014 Last visit: 10/14/2024 Posts: 33954 Rating: (4221)
|
Hello BereBonkerKING, at first welcome to the forum. In attachment a screenvideo and two LAD diagrams. The diagrams shows you how to make a master/master communication between two LOGO!s. One is the client (active part) and one is the server (passive part). AttachmentMaster_Master.zip (242 Downloads) |
3/24/2020 12:47 PM | |
Posts: 2 Rating: (0) |
Hello, Thanks for you answer and i see how i can cofigure it to simulate in network, but take a look at this screenshot. I can't import my ladder diagram into the logic module. Second question : With SFB you have acces to 400 blocks in the intern memory. Does this also count for ladder diagram? Greeting, Tim (BereBonkerKing) AttachmentSiemens.pdf (194 Downloads) |
Follow us on