4/14/2024 9:03 PM | |
Joined: 4/14/2024 Last visit: 4/29/2024 Posts: 3 Rating: (0) |
Hi I am also having similar issue on my atlas copco compressor GA45VSD fixed with the Elektronikon II with the siemens micro master 440. In my case i can start the compressor through the start button on the elektronikon II , but I can't stop the compressor through the STOP button on the Elektronikon II controller. The display on the module shows "PROGRAM STOP" but it is not stopping the compressor even after few minutes. In this condition, I am stopping the compressor by switching off the incoming breaker. Presently, i have the following set parameters on the MM440 (S/N: T-V611562000135) P0700=5,2,2 P1000=5,3,3 P0701=1 P0702=12 P1300=3,2,3 On MM440, they used DIN 1, DIN2 and termilal 29, 30(connection from Elektronikon II module RS485). I would be greatful if you help us to troubleshoot the issue. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/15/2024 06:42:51New subject after splitting |
|
4/15/2024 5:03 AM | |
Joined: 3/25/2008 Last visit: 7/28/2024 Posts: 192 Rating: (8) |
tell me what is the parameter set there? it is stuck on the converter
|
Follow us on