10/28/2014 9:43 AM | |
Joined: 3/19/2010 Last visit: 4/17/2024 Posts: 438 Rating:
|
Hello, I have Step 7 V5.5 SP4, and CFC 8.0 SP2. My CFC crashes in one very specific situation, otherwise it has been working very well for months, maybe two years. I have dowlnoaded function AR_BSEND, made by one of the forum members, the function is made in SCL, and here is the copy of it. When I drag this FB and drop it from the Blocks folder to my CFC chart, it crashes! Now, please read further. But, the same thing is working well when I try it on the different account on my personal laptop! I must say that both accounts are with Administrator privileges. It also works well on every other PC of my colleges I have tried on. I tried to reinstall completely Step7 and CFC, I tried with different versions and even older Service Packs, but nothing happened, the problem is the same. I don't know where else to look. Can somebody give me a hint why would possible the user account be responssible for CFC crashing? Why? There must be some privilege, or some service, or something very untrivial that I should look for. Something that CFC does when it wants to put the function in the CFC, some background procedure that I cant' figure out. AttachmentAR_BSEND.zip (129 Downloads) |
Follow us on