2/27/2019 6:50 PM | |
Joined: 9/27/2006 Last visit: 10/20/2024 Posts: 12289 Rating: (2688) |
Hello Milosh; To stop the master from polling the missing slaves, you cn: - reconfigure the Profibus network to remove the uninstalled slaves; - use D_ACT_DP (SFC 12 in Step 7 Classic) instruction to disable the polling of these slaves in the master's poll cycle. How do you enable and disable DP slaves and IO devices using the 'D_ACT_DP' instruction? https://support.industry.siemens.com/cs/ww/en/view/105020938 Hope this helps, Daniel Chartier |
Follow us on