8/9/2016 2:10 PM | |
Joined: 4/24/2006 Last visit: 7/4/2024 Posts: 8711 Rating:
|
Hello DesignTech, Please have a look at the following link: You can use SFC14 and SFC15. Best regards, Wizard |
8/9/2016 2:14 PM | |
Joined: 9/27/2006 Last visit: 7/4/2024 Posts: 12266 Rating:
|
Hello Design Tech; In the following FAQs you will find a sample configuration of a CP 342-5 as a Profibus slave (to a S7-300 CPU as master), and an explanation of DP_Send amd DP_Rcv functions required for cdata exchanges between the CP 342-5 and the CPU it shares the rack with (not the DP master on a seperate rack). DP link between CP 342-5 (slave) and S7-300/400 (master) with STEP 7 V5.1 https://support.industry.siemens.com/cs/ww/en/view/6519580 With the CP 342-5 you must always use the functions FC1 and FC2 for data transfer from the CPU to the CP... What should you watch out for when configuring a CP342-5 as DP master and why is it necessary to call the FC1 'DP_SEND' and FC2 'DP_RECV' functions in the user program of the CPU in order to transfer data? https://support.industry.siemens.com/cs/ww/en/view/18208090 Hope this helps, Daniel Chartier |
8/9/2016 2:15 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello, perhaps might help you: What master/slave communication options are available on ... - Siemens What are the options for exchanging data between CPUs ... - Siemens What are the differences between an integrated DP ... - Siemens |
8/9/2016 4:04 PM | |
Joined: 4/24/2006 Last visit: 7/4/2024 Posts: 8711 Rating:
|
Hello, I have two options: - S7 300 CP342-5 - CP342-5 (GSD file SIEM80D6) Best regards, Wizard |
Follow us on