12/21/2023 2:27 PM | |
Joined: 9/27/2006 Last visit: 11/6/2024 Posts: 12293 Rating: (2690)
|
Hello TEJCOOL; This application example will give you documention and a sample project for PUT/GET functions between 2 S7-300 CPUs. https://support.industry.siemens.com/cs/ca/en/view/82212115 Your S7-317 using a CP 343-1 must act as a client in ths project, while the S7-315 with a CP 343-1 LEAN must be configured as a server. Look at the documentation file, study the description of the S7-300 configurations. There is a chapter based on TIA Portel, another one on Step 7 v5.6,. Then select the appropriate sample program and use it to understand the configuration and programming of your CPUs. Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
12/21/2023 2:35 PM | |
Joined: 8/23/2022 Last visit: 3/1/2024 Posts: 3 Rating: (0) |
Hi Daniel, Thanks for the information! That was really helpful. |
Last edited by: TEJCOOL at: 12/21/2023 14:38:21 |
|
12/22/2023 6:46 AM | |
Joined: 7/9/2015 Last visit: 11/6/2024 Posts: 4019 Rating: (601)
|
Hi TEJCOOL, I can recommend you a very good manual. Please check table 21.4.2 S7300/S7-300 on PDF Page 103. Ther you can read, that in PLC with CP Lean is only server. CPU-CPU Communication with SIMATIC Controllers Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
Follow us on