10/4/2019 6:38 AM | |
Joined: 5/12/2006 Last visit: 10/18/2024 Posts: 22422 Rating: (3023)
|
hello, you can use the LCom Library or the Systemfunctions (xsend/xreceive, TCPsen/TCPreceive) manual communication with SIMOTION Regards Christoph |
10/4/2019 10:33 AM | |
Joined: 12/20/2012 Last visit: 8/4/2024 Posts: 57 Rating: (0) |
Dear ChristophD, Thanks for your reply. My project: S7-1500 is Master and Cimotion c240 is slave. thus is it need usd LCom Library or the Systemfunctions (xsend/xreceive, TCPsen/TCPreceive) for CIMOTION? or these Functions are need just for s7-1500(Master). and another question: 1.also SIMOTION variable's exported to Wincc are absolute only and no change to symbolic. 2.on Scout TIA variables are absolute only. 3.in addition how i can connect to SIMOTION with another HMI brand by Ethernet? Protocol(variabls are absolute)? 3. is it FM351 or CP343-1(a PROFINET Module) supported by CIMOTION C240? |
Follow us on