12/20/2014 12:18 PM | |
Posts: 72 Rating: (2) |
Dear friends, I’m try to communicate logo and s7 1200 plc. I can’t able to communicate. I’m using example manual I have done same setting but it’s not working. Apart from this need to do any settings. Kindly suggest me how to proceed. There is any other manual ???. AttachmentinfoPLC_net_08_Comunicacao_LOGO_com_S7-1200.pdf (386 Downloads) |
12/22/2014 8:59 AM | |
Posts: 72 Rating: (2) |
Hi Toeternietoe, Thanks for your replay, Logo I’m using is OBA7.ES4 Logo CPU when I check online show FW version its show OBA7.ES4 so keep same in my configurations. I’m using software TIA13 & logo soft V8.0 1214c CPU IP: 192.168.0.1 sub is: 255.255.255.0 Logo IP: 192.168.0.2 and Sub is: 255.255.255.0 My laptop address is: 192.168.0.100 and sub is: 255.255.255.0 I’m able to access from PC to both CPU (upload, download, online I have checked). also i have attached configuration kindly check. Attachmentconfig.zip (364 Downloads) |
12/22/2014 10:01 AM | |
Posts: 72 Rating: (2) |
hi, thanks for your replay, just we are using normel ethernet switch D-LINK not a router. |
12/22/2014 12:38 PM | |
Posts: 72 Rating: (2) |
hi, if there is any other manual reg this kindly send the link.or any other settings ? OBA7.ES4 it will support ???
|
12/26/2014 9:13 AM | |
Posts: 72 Rating: (2) |
hi, Thanks for your valuable replay I have enable protection. But I fount connection errorhere I have attached screen short kindly check and suggest me. Attachmenterror.zip (294 Downloads) |
12/26/2014 9:50 AM | |
Posts: 72 Rating: (2) |
Partner connection image shown question mark (?). It’s just image or need select file? Note: I just manual type LOGO! OBA7. |
Follow us on