12/27/2014 6:18 PM | |
Posts: 8 Rating: (0) |
Hi Murali, I can't know how you have configured the connection in de Logo! end, but usually S7-1200 act as a server and Logo! as a client, so you must disable option in "Active connection stablishment" (connection properties) at the S7-1200 side. I attachsome screen captures with a very simple sample (anly 2 bits one in each direction) connection between S7-1500 and Logo! 8. I hope it will help you. AttachmentS7-1500 & Logo!8.zip (331 Downloads) |
12/29/2014 9:29 AM | |
Posts: 72 Rating: (2) |
hi, can you please attach your programe it will help full. thanks
|
12/29/2014 1:32 PM | |
Posts: 8 Rating: (0) |
Hi, Of course, here you are! But remember this program is for Logo! 8 and S7-1500 so take it with a grain of salt! Good luck and have a nice day! Miguel AttachmentCommunication s7-1500 and Logo! 8.zip (322 Downloads) |
This contribution was helpful to1 thankful Users |
1/5/2015 2:08 PM | |
Posts: 72 Rating: (2) |
hi, Its working fine.. thanks for your kind support
|
1/8/2015 2:46 PM | |
Posts: 72 Rating: (2) |
hai, I just reset Logo and configure setting thats it communication is active here with i have attached configuration setting will use for TIA13 AND LOGO! SOFT 8
AttachmentS71200_V13_logo_V8.pdf (320 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on