11/16/2022 7:14 AM | |
Joined: 7/31/2021 Last visit: 4/10/2023 Posts: 1 Rating: (0) |
I want to communicate my pc with Cp5622 and wincc flexible 2008 sp5 but when i test my profibus in simatic net pg/pc i get error "system error:device not available (41323)" ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/16/2022 11:07:00New subject after splitting |
|
11/16/2022 3:34 PM | |
Joined: 5/6/2022 Last visit: 5/21/2024 Posts: 420 Rating: (83) |
HiALIHbili, Could you tell me if your PC recognises the card from the device manager? On the other hand, here is a link to a FAQ where you can check the compatibility of windows with your card (as it could be that it is not compatible) and in this same Excel compatibility is indicated by operating system (OS) link to download the driver you would need. "Which SIMATIC NET PROFIBUS PC CP is compatible with which Microsoft Windows operating system?" Best regards! |
If this Information really helps, you could use the Rate function |
|
Follow us on