6/8/2017 11:17 PM | |
Posts: 23 Rating: (0) |
dear people. tank you so much for everything and you help. in this time i have this problem: i have this network attach 1. first: i used the SCALANCE W700 client 734-1fx00-0ab0 And is connected to the cpu s7 1500 i used the SCALANCE W700 ap 774-1fx00-0ab0 and is conected to the HMI KPT 700 BASIC PN and this work fine. second: i used the SCALANCE W700 client 734-1fx00-0ab0 And is connected to the cpu s7 1500 i used the SCALANCE W700 ap 774-1fx00-0ab0 and is conected to the ET200 And the connection fails third: i used the SCALANCE W700 client 734-1fx00-0ab0 And is connected to the cpu s7 1500 i used the SCALANCE W700 ap 774-1fx00-0ab0 and is conected to the RF180C And the connection fails fouth: i used the SCALANCE W700 client 734-1fx00-0ab0 And is connected to the cpu s7 1500 i used the SCALANCE W700 ap 774-1fx00-0ab0 and is conected to the sinamics s110 And the connection fails. please help me for this, why if worked with HMI KPT 700 and dont work for the others elements?. pd: I parametrize the balances by means of the static ip. tank you for your help, regards. Attachmentattach_1.pdf (427 Downloads) |
6/12/2017 9:14 AM | |
Posts: 1368 Rating: (126) |
Hello, the FAQ is not the newest, but it explains the way to increase the watch dog time TIA-Portal https://support.industry.siemens.com/cs/ch/de/view/109475919 STEP 7 V5.5 https://support.industry.siemens.com/cs/ch/de/view/109474533 |
This contribution was helpful to1 thankful Users |
6/16/2017 6:34 PM | |
Posts: 23 Rating: (0) |
hello dear and than you for everything help, in the attach i exposed my case. I can not establish communication between the cpu and the et200 per wlan or any other field device. i follow your advice, but they are still without communication. thank you again for everything. regards. pd: i actived the iFEATURES in the AP and client "iPCF". AttachmentERROR COMUNICATION PROFINET WLAN.pdf (441 Downloads) |
6/19/2017 11:14 AM | |
Posts: 1368 Rating: (126) |
Hello, do you also check PROFINET name of ET 200? Do you assign the correct name to the Device? And please look at this document: find on this entry https://support.industry.siemens.com/cs/ww/en/view/22681042 |
3/1/2023 10:26 AM | |
Joined: 11/13/2011 Last visit: 8/23/2024 Posts: 18 Rating: (0) |
Hello, Have you solved your problem? If yes, how ? Eric |
Follow us on