5/15/2024 7:52 AM | |
Joined: 6/10/2022 Last visit: 5/15/2024 Posts: 2 Rating: (0) |
Hello everyone, I have recently bought a ATLAS COPCO gateway MK5 and I need to connect it to a Siemens S7-1500 via PROFIBUS but I'm not able to establish the communication (the profibus node is not recognised by the PLC). The system that I have is the following: a Leybold Coolpak5000 connected via a CAN interface to the gateway (communication is ok for these two) and the gateway connected via profibus to the PLC (communication is not working). I received the GSD file from Leybold then I hope it is ok. I fear that I'm missing some simple configuration step: please, can you help me with a step by step guide to establish this communication? Thank you in advance. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/15/2024 08:46:43New subject after splitting |
|
5/15/2024 9:33 AM | |
Joined: 3/11/2019 Last visit: 6/21/2024 Posts: 1482 Rating: (267)
|
Hi mirkoc88,
Did you already install the GSD file and configured the gateway via this GSD in hardware config? If there are any specific issues right now, which ones? In general: regards sancruz |
Feedback appreciated, please rate |
|
Follow us on