9/24/2014 9:19 AM | |
Joined: 12/12/2011 Last visit: 11/13/2024 Posts: 69 Rating: (1) |
i have one problem. i using C240 controller (6AU1 240-1AA00-0AA0). For commisoining project, I connected C240 X7 enthernet to Switch Enthernet, then PC connected enthernet cable to this Switch Enthernet. Now i want use HMI WinccFlexible runtime on PC with C240. so it cannot connect betwen C240 with WinccFlexible Runtime via Enthenet connection. please give me your advice. if it can connect betwen C240 to WINCC Flexible Runtime on PC! Thank you! AttachmentHwsite_24Sep14.zip (286 Downloads) |
Last edited by: Min_Moderator at: 9/24/2014 1:10 PMLast edited by: Min_Moderator at: 9/24/2014 1:09 PMNew subject after splitting from /tf/WW/en/Posts/114741#top Last edited by: Min_Moderator at: 9/24/2014 12:06 PMUpload attachment |
|
9/24/2014 9:44 AM | |
Joined: 5/12/2006 Last visit: 11/14/2024 Posts: 22452 Rating: (3030)
|
Hello, which error do you get when WinCC Rt will connect to the C240? Regards Christoph |
9/24/2014 9:45 AM | |
Joined: 12/12/2011 Last visit: 11/13/2024 Posts: 69 Rating: (1) |
Hi ChristophD, No error, Wincc Flexible can not display Value from C240 on Scrreen. (#####). Thank you!
|
Follow us on