4/24/2015 7:35 AM | |
Posts: 5 Rating: (0) |
hello, i have a program in stl and i can use it with s7-300-400 or s7 1500 but i cant use it with s7 1200 as s7 1200 does not support stl so i want to convert it to fbd but dont know how to use LAR1 statement in fbd is there anyone who can help? LAR1 #Laddr //Open pointer in address register 1 L W [AR1,P#0.0] //Open first word T #DBE.word_0 //and save in DBE structure L W [AR1,P#2.0] //2. .... T #DBE.word_1 L W [AR1,P#4.0] T #DBE.word_2 L W [AR1,P#6.0] T #DBE.word_3 JU Net2 ---------------------------------------------------------------------------------------------------- Split from Pointers _ STL. |
Last edited by: Min_Moderator at: 4/24/2015 9:42:36 AMNew subject after splitting |
|
4/24/2015 9:54 AM | |
Posts: 5 Rating: (0) |
Attachmentsource.rar (85 Downloads) |
4/24/2015 9:55 AM | |
Posts: 5 Rating: (0) |
i sent also full program in step 7 for s7-300 cpu.. thanx in advance AttachmentArcelik_.zip (86 Downloads) |
4/25/2015 11:04 AM | |
Posts: 5 Rating: (0) |
thanx a lot |
This contribution was helpful to1 thankful Users |
2/6/2017 3:20 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by Pramod26 is split to a separate thread with the subject Help in understanding STL program. Best regards |
Follow us on