6/19/2012 6:05 PM | |
Posts: 1547 Rating: (129)
|
Hi, if there are no big secrets in your project you could archive it and post it here. With some luckthere is a simple solution to your problem. |
6/20/2012 11:39 AM | |
Posts: 20 Rating: (0) |
No, there is no secret at all in that project . It is just a test for some gaining in experience. Attached are two different projects. Both were approaches to get it working..and both failed . As mentionend before I can't couple the CP1616s and I can't assign the transfermoduls of the CP1616-Routing-Device with the I/Os of my actual IO-device (grayed area/empty). AttachmentIO-Router.zip (266 Downloads) |
Last edited by: JimBeam at: 6/20/2012 11:40 AM |
|
6/22/2012 11:27 AM | |
Posts: 20 Rating: (0) |
Sorry to bother you again, but the OPC-Stuff still doesn't work. I finished the project (see attached procjet folder in the archive), downloaded it into the PC-Station with the CP-1616, imported (Import Station) it into the PC-Station with the OPC-Server (another PC in the same network) and created the items in OPC-Scout. Exactly the configured transfermoduls are showing up in the OPC-Item tree, so the station import seems to have worked (see attached screenshot 1 in the archive). But the OPC-Server showed just an invalid item-status (see attached screenshot 2 in the archive).. I guess that there is no connection. Pinging of all network participants works on both PC-Stations. What shall I do now? AttachmentOPC-Problem.zip (289 Downloads) |
Follow us on