4/16/2011 6:43 AM | |
Joined: 1/21/2011 Last visit: 1/23/2024 Posts: 162 Rating:
|
Hi i have problem in the cp1616 interface card (partno:6GK1161-6AA01) while inserting the card in the industrial pc it affect the tcp/ip connection ipaddress it shows blank some time it shows error message . screen shot is in attach file. regards k.jagan Attachmenttcip.pdf (243 Downloads) |
4/18/2011 9:19 AM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating:
|
There's a kind of bug from Windows in combination with the RTX part, if you move the network adapter from Windows side to RTX side. Windows seems to have problems with it. See manual for WinAC RTX http://support.automation.siemens.com/WW/view/en/43715176 , chapter 12.3.3. There is a part given telling something about using several Ethernet interfaces which gives you some help on it. |
Have Fun! |
|
Follow us on