11/22/2012 8:42 AM | |
Posts: 4 Rating: (0) |
Hi, Has anybody experience using datalog new file? I have a problem with it.. At first I use Version V11 SP2 Update 4. I have buid it my program as follows: -create,write and when the write block is full then I try to make a newfile. The problem is how I get it the full status bit which makes the newfile. My write block always overwite the datarecord and I don't want it. So I get always error 8093 (datalog already exist).And if I close the datalog I get error 80B0 (datalog file isn't open) Look attachments there are how the write blocks have done and errors. If possible give me example or something... Attachmentnewfile.zip (324 Downloads) |
Last edited by: Juve12 at: 11/22/2012 10:51 AMLast edited by: Juve12 at: 11/22/2012 8:49 AM |
|
Follow us on