7/4/2013 12:18 PM | |
Posts: 1064 Rating: (72) |
another thing to check is that with wincc in runtime hoover your mouse over the tag and check the valueto make sure you are connected and it is a valid dbw |
7/4/2013 12:31 PM | |
Posts: 2 Rating: (0) |
Thanks for your answer. Where would i set the 16bit unsigned? As far as i can tell i can only set tags to fixed data types like INT, Word, DWord, etc. |
7/4/2013 1:07 PM | |
Joined: 10/3/2010 Last visit: 5/29/2024 Posts: 1552 Rating: (188) |
did you check your Output Format-property of the I/O-field? You can also get '#########' whenever the actual value doesn't fit in your configured Output Format. |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
Follow us on