9/9/2020 12:54 PM | |
Posts: 4 Rating: (0) |
Hi everyones I've got recently a logo 0ba0 and i have some trouble to upload my web server on it I've uploaded the file on the SD car using "Deploy to SD card" Ive activated the WebServer acces thru the settings of the logo! Now the SD card is back into the logo! but when come the time to upload the project using the "Upload" button i get the error "Download Failed! There is no file system in SD Card" I need some help ! Ty vm ------------------------------------------------------------------------------------------ |
Last edited by: phong19961223 at: 09/09/2020 12:56:03Last edited by: Jen_Moderator at: 09/09/2020 13:38:38New subject after splitting |
|
9/10/2020 3:22 AM | |
Posts: 4 Rating: (0) |
I did SD card be formatted with FAT32 and i get the error "Download Failed! There is no file system in SD Card" |
9/10/2020 3:47 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33499 Rating: (4162)
|
|
9/10/2020 3:56 AM | |
Posts: 4 Rating: (0) |
|
Last edited by: phong19961223 at: 09/10/2020 04:03:19 |
|
9/10/2020 3:58 AM | |
Posts: 4 Rating: (0) |
micro sd card read error |
Last edited by: phong19961223 at: 09/10/2020 04:04:27 |
|
9/10/2020 4:20 AM | |
Joined: 12/18/2014 Last visit: 8/7/2024 Posts: 33499 Rating: (4162)
|
Attached a photo of a SD card slot where the pins are bent. |
Follow us on