11/1/2016 4:58 PM | |
Joined: 3/28/2015 Last visit: 5/25/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help: 1-How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? 2-In WinCC (TIA Portal), how do you transfer a project to an HMI panel using S7 Routing? "The download of a WinCC (TIA Portal) project from the configuration computer to a panel should not be made via a direct connection but via an S7 routing with an S7 CPU connected in between". |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
Follow us on