3/21/2020 9:26 PM | |
Posts: 7 Rating: (0) |
Hi friends. I have the same problem. I downloaded Backup from the OP7 panel with Prosave. The program cannot see this file. Protool whether it is SP1, SP2 or SP3. (there are some problems with installation SP3) As the file sees, it can not be convertet because it reported thats it was created in wersion 1.x. How to solve it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/23/2020 06:44:44New subject after splitting |
|
3/21/2020 11:18 PM | |
Joined: 9/27/2006 Last visit: 11/18/2024 Posts: 12294 Rating: (2691) |
Hello Yano; I have no idea if this download will be able to help you: Download: ServiceTool ProSave V1.1 https://support.industry.siemens.com/cs/ww/en/view/11017496 This is a DOS file, for starters, you will have to use a PC that is able to run it, either directly ion a DOS setup or partition or in a Command Prompt window..And you must use a cable that connects to an actual COM port. Second, what panel (exact part number and version) are you attempting to download this to? You do know that a Prosave file cannot be opened in ProTool for verification or modification, it can only be downloaded to an exact match of the original panel... Hope this helps, Daniel Chartier |
Follow us on