11/18/2015 10:38 PM | |
Joined: 6/4/2008 Last visit: 7/18/2024 Posts: 1485 Rating:
|
Hi again, the only downloads for firmware on the Siemens site are v3.33 and v3.4. I would advise against going to that high a version on that old card, although I'm not sure if it would work or not - call it a gut feeling. I will attempt to attach a v3.13 firmware patch to this reply, but it may get removed as it has exe's and bin's in it. You will need to run it in Win XP and it is a command line version. The windows versions "WinBSL" came later on. Please do scan any attached files from ANY user on here - we are all fallable. Don't forget your bootstrap cable to flash firmware, you should see the 'E' on the PMU when ready to accept new firmware Last but not least, whilst I don't want to dampen your enthusiasm, this is AT YOUR OWN RISK Regards, Graeme Attachmentvc_v313.zip (670 Downloads) |
1/28/2019 3:43 PM | |
Joined: 6/19/2018 Last visit: 3/18/2024 Posts: 22 Rating:
|
Hi all, I know that this thread is very old, but we had the same problem in our Masterdrives last week. The problem started because we could't connected to the previous version of drive monitor with our PG. So we update the drive monitor after that we connect, but the unit type and version fields was just '????'. So we found a TXT that I'm attach with the instructions to update the firmware and build the wire to update it. Downloaded the latest version of CUVC firmware for our CUVC. And after the update everything was work correctly. regards
AttachmentREADMEVC.DOC (741 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on