6/7/2011 10:08 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Please check the following Software (Desklock) which is a powerful software to just provide limited and authenticated permission to Windows' combination keys and all possible administrators' duties are controlled by a password and also you can also define start up programs. It worths testing. regards |
6/9/2011 8:19 AM | |
Joined: 10/3/2010 Last visit: 9/30/2024 Posts: 1562 Rating: (192) |
entry 44027453: How can you lock key combinations in WinCC V7.0 SP2 with Windows 7 or Windows Server 2008? http://support.automation.siemens.com/WW/view/en/44027453 |
B r g d s , |
|
9/10/2012 3:17 PM | |
Posts: 1776 Rating: (95)
|
Hi, see the link SteBo published |
4/23/2013 2:47 PM | |
Posts: 767 Rating: (69) |
Hello, I'm also looking for an option to enable key combinations during runtime. Normally the key combinations have to be disabled. I want toenablethemto help the engineers during service. With windows XP and 2003 the following solution works: http://support.automation.siemens.com/WW/view/en/22326550 But this doesn't work with windows 7 . Is there anyone who has an solution for Windows 7???? Thanks in advance! Cedric |
4/24/2013 10:59 AM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Hi Experts, I also tried the solution SteBo provided: http://support.automation.siemens.com/WW/view/en/22326550 It should work with Win7 but itdoesn't. I tried to debug but it seems to work fine,but nolock or unlocking of the taskbar. Hope you can help out Jaap I used this script, it triggers fine and state switches from enable to disable but whithout any result. maybe it's an security setting in Windows?: #pragma code ("UseAdmin.DLL") #include "pwrt_api.h" #pragma code() #pragma code ("ALMXGINA.DLL") BOOL SetXGinaValue(unsigned int uiKey, BOOL *pbEnable, DWORD dwSize); #pragma code() BOOL bEnable; BOOL bOK; #define XGINA_ALLOW_SHUTDOWN 1 #define XGINA_ALLOW_LOGOUT 2 #define XGINA_ALLOW_CTL_ALT_DEL 3 #define XGINA_ALLOW_CTL_ESC 4 #define XGINA_ALLOW_ALT_ESC 5 #define XGINA_ALLOW_ALT_TAB 6 bEnable = PWRTCheckPermission(1, TRUE); bOK = SetXGinaValue(XGINA_ALLOW_SHUTDOWN , &bEnable , sizeof(bEnable )); bOK = SetXGinaValue(XGINA_ALLOW_LOGOUT , &bEnable , sizeof(bEnable )); bOK = SetXGinaValue(XGINA_ALLOW_CTL_ALT_DEL , &bEnable , sizeof(bEnable )); bOK = SetXGinaValue(XGINA_ALLOW_CTL_ESC , &bEnable , sizeof(bEnable )); bOK = SetXGinaValue(XGINA_ALLOW_ALT_ESC , &bEnable , sizeof(bEnable )); bOK = SetXGinaValue(XGINA_ALLOW_ALT_TAB , &bEnable , sizeof(bEnable )); printf("#I101: SetXGinaValue() - bEnable=%d bOK=%d (lock/unlock windows keys)\r\n", bEnable, bOK); |
Follow us on