6/26/2024 3:39 AM | |
Joined: 6/12/2024 Last visit: 7/2/2024 Posts: 2 Rating: (0) |
Hi, I installed TIA Portal V19 with all other software including WinCC Basic/Confort/Advanced and Win CC Professional and Win CC Unified, no issue at all. I have not activate yet. After I installed, I will activate Win CC RT Professional V19. When I install Win CC RT Professional V19, I have the error as per the attahced file and I cannot able to install. See attached Zip file for all error screenshots and error file. Please help!!!. 17:17:35 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error <https://support.industry.siemens.com/cs/ww/en/ps/14667/faq> 17:14:27 | BEGIN. Execution started. 17:14:34 | OK RunningProcesses () Complete 17:14:34 | OK InventoryBefore (A) Complete 17:14:34 | OK Citamis (Before) Complete 17:14:50 | OK SecurityControlFeature (ReturnFeatures) Complete 17:14:50 | OK ClassicCompPrepare () Complete 17:14:50 | OK ProductRegistration (Before) Complete 17:14:50 | OK ClassicCompAfterUninstall () Complete 17:14:50 | OK SetupUnit (DotNet_Updater) Complete Foreign AddLocal 17:14:50 | OK Checkpoint (RE) Complete 17:14:50 | OK SetupUnit (SQLNCLI) Complete Foreign Reinstall 17:15:15 | OK SetupUnit (INSTSQL2019STD) Complete ClassicProductReinstall 17:15:15 | OK Checkpoint (E) Complete 17:15:15 | OK SetupUnit (SYMLINK) Complete Foreign AddLocal 17:15:17 | OK SetupUnit (SYMLINKADD) Complete Foreign AddLocal 17:15:18 | OK SetupUnit (OPCCORECOMP64) Complete Foreign Reinstall 17:15:18 | OK SecurityControl (WinCC ACE) Complete 17:16:44 | OK SetupUnit (WinCC ACE) Complete ClassicComponentReinstall 17:16:47 | OK SecurityControl (WinCC ACE) Complete 17:17:34 | OK SetupUnit (WinCC Common Archiving) Complete ClassicComponentReinstall 17:17:35 |ERROR AdsWorkerClassicComponent::OnWorkerCompleted(): - ClassicProduct setup failed due to unknown error 17:17:35 | FAIL! SetupUnit (OPC) Failed ClassicComponentAddLocal 17:17:45 | OK SetupUnit (Runtime Interfaces) Complete ClassicComponentReinstall 17:17:51 | OK SetupUnit (HMIProvider) Complete ClassicComponentReinstall 17:17:59 | OK SetupUnit (SECON) Complete ClassicComponentReinstall 17:17:59 | OK Checkpoint (R) Complete 17:18:07 | OK SetupUnit (S7EDB) Complete ClassicComponentReinstall 17:18:22 | OK SetupUnit (PTSymLib) Complete ClassicComponentReinstall 17:18:30 | OK SetupUnit (PTTouchInput) Complete ClassicComponentReinstall 17:18:44 | OK SetupUnit (STOBS) Complete ClassicComponentReinstall 17:18:45 | OK SecurityControl (LicenseManager) Complete 17:19:21 | OKRebootAfterAll SetupUnit (LicenseManager) Complete ClassicProductReinstall 17:19:23 | OK SecurityControl (LicenseManager) Complete 17:19:24 | OK SecurityControl (SCADA-RT) Complete 17:21:08 | OKRebootAfterAll SetupUnit (SCADA-RT) Complete PlusMain Reinstall 17:21:18 | OK SecurityControl (SCADA-RT) Complete 17:21:22 | OK SetupUnit (RT_Pro) Complete PlusOptionalReinstall 17:21:23 | OK SecurityControl (OPC-Server) Complete 17:21:27 | OK SetupUnit (OPC-Server) Complete PlusOptionalReinstall 17:21:29 | OK SecurityControl (OPC-Server) Complete 17:21:29 | OK SecurityControl (OPCUA_Client) Complete 17:21:34 | OK SetupUnit (OPCUA_Client) Complete PlusGlobalReinstall 17:21:34 | OK SecurityControl (OPCUA_Client) Complete 17:21:38 | OK SetupUnit (DocuViewer) Complete PlusGlobalReinstall 17:21:54 | OK SetupUnit (WinCCTools) Complete ClassicProductReinstall 17:21:54 | OK ClassicCompAfterInstall () Complete 17:21:54 | OK ClassicCompRollback () Complete 17:21:54 | OK HspInstall () Complete 17:21:54 | OK MspInstall () Complete 17:21:55 | OK ProductRegistration (After) Complete 17:21:57 | OK SetupIsComplete () Complete 17:21:57 | OK InventoryAfter (Z) Complete 17:21:57 | OK LicenseTransfer (False) BeforeStart 17:21:57 | OK Citamis (After) Complete 17:21:58 | OK SetupSummary () Complete 17:23:36 | OK SetupReport () Complete 17:23:36 | END. Execution completed. Intermediate ExitCode after execution queue : 1603 - Exit code means: Installation failed (InstallFailure) Errors: 1 Warnings: 0 [attachment id="9749" /] [attachment id="9750" /] [attachment id="9748" /] ------------------------------------------------------------------------------------------ AttachmentError.zip (32 Downloads) |
Last edited by: Mikedot9988 at: 06/26/2024 03:42:46Last edited by: Mikedot9988 at: 06/26/2024 03:44:06Last edited by: Mikedot9988 at: 06/26/2024 03:44:37Last edited by: Jen_Moderator at: 06/27/2024 07:10:59New subject after splitting |
|
Follow us on