1/7/2016 8:09 AM | |
Posts: 153 Rating: (9) |
Hello I connected a simotion d435 4.1 and s7315-2pn/dp via profibus i can send a data to simotion, but i can only run and stop 1 time, it appear a error missing enable parameter 1:7 and/or incorrect mode parameter 2:1 it only appear when i enable axis by ENABLE_BIT which is send from PLC, when i use glori variable ENABLE_MCC erorr not appear Please tell me how can i fix it thank you, the project and error picture is blow Attachmenterrorr.zip (60 Downloads) |
Last edited by: KhanhLe at: 1/13/2016 8:56:36 AMLast edited by: KhanhLe at: 1/13/2016 8:57:24 AM |
|
Follow us on