5/2/2023 9:01 AM | |
Joined: 4/24/2023 Last visit: 4/30/2024 Posts: 4 Rating: (0) |
Hello! I probably try to use similar solution what was offered but beside the relay solution I have a question: If I select PTO I can select between all the PLC I/O-s and signal board I/O-s Do I still need to make some separation with relays? If my 2 axis are configured for differnt I/O then I just position axis1 for example (using PTO1) then release axis (release PTO1). Enable second axis (using PTO1 with differnet output channel) position the eaxis and power it Off (release PTO1) could this logic work wo relay schematic? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/02/2023 12:36:57New subject after splitting |
|
5/3/2023 10:36 AM | |
Joined: 3/30/2020 Last visit: 11/7/2024 Posts: 4932 Rating: (1008)
|
You will have to evaluate the following idea.. Assume there are 8 axis which can be grouped in 2 groupings (A and B). Only one motor from a grouping can run at a time. Stepper A1 (motor 1 of grouping A) and stepper B1 cannot work at the same time. A1 and B1 however share Q0.0 and Q0.1 which is the pulse-and-direction pair. Both A1 and B1 is wired to Q0.0 and Q0.1. Q0.0 and Q0.1 is declared as PTO1 and controlled by the technology object "AxisAB1". The enable output of "AxisAB1" is routed to memory bit M0.0. A1 and B1 has different enable signals, respectively sourced from Q2.0 and Q3.0. The state of M0.0 will switch Q2.0 or Q3.0 depending on which motor is scheduled to run. When switching from A1 to B1 the following happens:
EDIT (a) Using multiple axes with the same PTO |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
5/5/2023 5:49 AM | |
Joined: 4/24/2023 Last visit: 4/30/2024 Posts: 4 Rating: (0) |
Thanks for your reply. I will try out the solution and post a feedback after few months how did it went
|
Follow us on