11/13/2009 10:34 AM | |
Posts: 3 Rating: (0) |
Dear all, I've a master drive , used in Motion control with a servo motor ,the drive begin to show F008 which is dc undervoltage I've checked almost every thing ,i can't find any reason for this. I've changed the drive itself with a spare one i've imported the parameters and downloaded it the spare one the machine worked for 10 days then stopped. I've changed the motor ,same fault. Even the line filters . some times the it shows an overvoltage with 16000 !!!!!!!! vdc how could this be??! the machine has been working for about 8 years till now. I've attached file for drive monitor for all parameters can any body help me??? Regards Simon Attachmentmaster parameter.zip (154 Downloads) |
Follow us on