4/2/2019 8:15 AM | |
Joined: 1/24/2012 Last visit: 1/9/2024 Posts: 16 Rating: (1) |
Hi, Dear Experts, I used the Siemens "Create_S7DB" excel file to create the automatic DB on simatic manager 5.6sp1. but, while opening the excel file i'm facing the below issues. 1. while opening excel its showing 2 pop-up a)"Couldn't load some objects because they are not available in this machine". b)"Please install Step7 or modify Autoexec.bat: SET PATH= %PATH%;DRIVE:\SIEMENS\STEP7\S7BIN;" 2. step7 simatic manager v5.6sp1 and MS-excel is already installed in the same PG. please help me to resolve this. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/2/2019 12:42:05 PMNew subject after splitting |
|
4/5/2019 10:33 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (133) |
Hello Vijay.k, check whether the internal STEP 7 database was started when the PC was booted and also the function Start/stop server in the SIMATIC workstation. For this, in Windows you open the dialog "Start > SIMATIC > STEP 7 > Configure SIMATIC workstation". In order to be able to start the internal STEP 7 database, the following entries must be available and executed in the autoexec.bat in Win95/98:
There is an application in the internet with the example “Automatic generation of an S7 data block with STEP 7 V5.x from an MS Excel 2003 table”. Perhaps it could be meanful for you. https://support.industry.siemens.com/cs/ww/en/view/15162450 Cicero |
Last edited by: Cicero at: 4/5/2019 10:35:14 AM |
|
7/3/2021 6:08 AM | |
Posts: 25 Rating: (2) |
Hi VIJAK
|
8/4/2022 8:56 AM | |
Joined: 1/2/2014 Last visit: 5/24/2024 Posts: 142 Rating: (22) |
|
Follow us on