5/22/2024 12:55 AM | |
Joined: 9/17/2023 Last visit: 5/22/2024 Posts: 1 Rating: (0) |
Hi everybody! I'm using a 1511T-1 and i'm trying to write data to an IO-Link Device (Balluff Sensor Hub - BNI005P - BNI IOL-104-S01-Z012-C02) using a module SMC IO-Master ( EX600-LAB1) connected on a SMC Profinet Interface (EX600). To do so I'm using LIOLink_Device FB from Siemens library: https://support.industry.siemens.com/cs/br/pt/view/82981502/en Doesn't matter what I do, I always get an error 8601 - Diagnostic C080_B200. I tried to find what this means but can find it anywhere. The configs im using on the block are: HwID: I'm using the ID of my Master IOLink (tried also with the ID of the port) Cap: Tried 0, 255, 16#B400, 16#00E3. readWrite: 1 Port: 4 (it is on C3 - on the block is from C0 to C3. Also tried with ports from 0 to 4) Index: 96 ( Want to write on the index 60hex) Subindex: 0 writeLen: 4 I Also attached some images with my configs. Do you have any clue what can I be missing? Thanks! Attachmentimages.zip (372 Downloads) |
Last edited by: Jen_Moderator at: 05/22/2024 09:42:48Text formatting and link optimized. |
|
This contribution was helpful to1 thankful Users |
Follow us on