5/18/2017 5:43 PM | |
Joined: 4/30/2007 Last visit: 3/9/2023 Posts: 231 Rating: (23) |
Question, Is it possible to find out the calculated Update time if the device was set Automatic? in an existing installation, most of the devices were set to Automatic "Automatic": With this, you select an automatically calculated and reliably achievable update time based on the configuration of the IO system. The project in question has more than 140 devices, and I would like use the Network load calculation tool (from PI) for the load calculation, however is necessary as input the Update time ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/19/2017 12:22:30 PMNew subject after splitting |
|
Follow us on