3/29/2009 11:50 AM | |
Posts: 103 Rating: (11) |
how are all , AttachmentSQL 2005 error.zip (160 Downloads) |
3/30/2009 7:27 AM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242) |
Hi, Is there any other SQL instance installed on this PC ? |
Best regards, |
|
3/30/2009 8:31 AM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating: (136)
|
hello together, maybe this thread is helpfull: /tf/WW/de/Posts/24294 do you have installed Windows XP SP3 ? because i heared that SP3 give problems with installing SQL Servers... And what about your system? is it the real systemdate? If not, then change ist to 2009. i hope i could help you... |
3/30/2009 4:21 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Or... Is the WMI service started? Run "wmimgmt.msc" to check... Hope this will helps. Best regards |
3/31/2009 10:17 AM | |
Posts: 103 Rating: (11) |
I want to thank you UMENCHO, when I try to run wmimgmt.msc the PC displays error ,the picture of error in the attachment but I choose the 3rd choice , when I try to make setup again , the same error occurs . please be in contact with me till solve this problem . thank you Attachmenterror.zip (153 Downloads) |
3/31/2009 1:14 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Ahmed, If the problem still exist look at -
Read the forum thread on the following site: http://forums.microsoft.com/MSDN/Sho...93534&SiteID=1 Then try to install SQL Server. Hope this helps. Best regards |
3/31/2009 1:38 PM | |
Posts: 103 Rating: (11) |
many many many thanks the code you wrote operates properly , my problem solved . thaaaaaaaaaaaaaaank you alot |
Follow us on