9/24/2014 7:39 AM | |
Joined: 5/19/2011 Last visit: 8/22/2023 Posts: 196 Rating: (5) |
Please reply to this thread i am stuck. |
9/24/2014 10:51 AM | |
Joined: 5/19/2011 Last visit: 8/22/2023 Posts: 196 Rating: (5) |
Hello piscean, Thanks for the reply. How many axes are configured?-Total 6 axis (X1X2,Y1Y2,Z1Z2-leading & followng) Issingle axis driven by individual motor -All motor are driven by separate servo motor-With common mechanical coupling What do you mean by change in sequence? -I want to give some movement to Z1Z2(Up/Down) axis in order to accomodate my new job(part) in the press. In existing scheme PLC send the data postion setpoint with feed to NC through Ncvar block Is this press, hydraulic or mechanical?-Mechanical press driven by servo motor having encoder feedback. I wanted to know how the axis are moved if the CNC part program is not running when i go to online through HMI advanced since the machine is customized OP37(protool). How the axis are positioned? Part program is used for referncing & synchronizing the gantry axis. I am attaching the PLC backup for the same in that FB171 & FB172 are used for reading & writing the NC parameters. Attachmentpress.zip (209 Downloads) |
Follow us on