1/9/2011 4:56 AM | |
Posts: 12 Rating: (0) |
Dear Miltos, I thank you for giving me your time. I'll keep that i mind Thanks for the info. Best Ragards.. |
1/10/2011 12:08 PM | |
Joined: 9/6/2008 Last visit: 3/29/2024 Posts: 134 Rating: (16) |
in similar case ,i use an digital intstument from Omron ,that have the posibility to receice and filter the singal from load cell-s ,and is full programiable for the outpout. at the same time is also a display,and i have used until now ,in more than 50 packing machines check the manual. Attachmentk3hb-v_dsheet_csm264.pdf (187 Downloads) |
http://electrotech-techblogg.blogspot.gr/ |
|
This contribution was helpful to1 thankful Users |
1/10/2011 8:52 PM | |
Joined: 3/4/2009 Last visit: 10/28/2020 Posts: 57 Rating: (5) |
I have also used such a module (this one: http://www.pgmavridis.com/english/weighm1.htm) There is nothing nothing strange with those modules. But i wonder how does the output signal of the loadcell (max 2mV/V --> 0-10mV or 0-20mV) arrive to the module without disturbances. I was supprised from that fact. |
Last edited by: miltos at: 1/10/2011 8:58 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on