9/11/2008 2:13 PM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
You have to build the required function your self. But what do you meant by "several setpoints?" |
Ayman Elotaify |
|
9/11/2008 3:09 PM | |
Posts: 2930 Rating:
|
Hi, For your time switch the best example you can get from: www.s7-200.net Her you can download free of charge Libraries from LOGO! functions translated to S7-200 code. I'm not a HVAC specialist but as I understand your heating systems: 1. The indoor heating does only switch on if the outside temp. is < then 17° cel. 2. The indoor temp you can controll via S7-200 PID control function. Use the Wizard in Micro/WIN for configuration. 3. A application like this normaly also requires a scalling funktion. Here is an example: To import it to Micro/WIN see the online help. I hope this helps. Regards Helmut AttachmentScaling.zip (235 Downloads) |
9/12/2008 10:59 AM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
closed cause question posted twice. The second thread with the subject Heating Optimum Controlis published within the same conference . Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on