8/2/2022 10:29 AM | |
Joined: 5/30/2022 Last visit: 9/20/2024 Posts: 581 Rating: (96) |
Hi xmnj, I think the best option is to store the alarms in a .csv file as shown in the following guide: https://support.industry.siemens.com/cs/ww/en/view/32947964 I also recommend you review the following information in case it is useful to you: |
If this information really helps, you could use the Rate function. |
|
8/2/2022 10:41 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Hi Hazard_7, Thank you for answering. I don't really want to store the Alarm Texts any other places than where there are stored now (in the project which is backed up by VersionDog) What I want to do is send the modify the Alarm List (I know how to do that) and send the modified List to where the texts in the List is displayed on the screen. Are you saying that the Alarm List must be downloaded to the panel NOT to the PLC? I hope I can find some of the information I am needing in the manuals you included links for.
|
8/2/2022 10:59 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello xmnj, Perhaps this might help: SIMATIC Programming with STEP 7 See chapter 16 Best regards, Wizard |
This contribution was helpful to2 thankful Users |
8/2/2022 1:15 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hi, Did you have a look at chapter 16.7? Best regards, Wizard |
This contribution was helpful to1 thankful Users |
8/3/2022 7:38 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Hi again Wizard, I thought I did but obviously not well enough - I apologize. However I am not quite there yet - I cannot find the "AS - OS Connection Data" the manual mentions? (AS - OS Engineering IS installed).
AttachmentAlarmlist A.zip (558 Downloads) |
8/9/2022 2:37 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Is there really no one that can answer this? |
Follow us on