7/12/2021 10:58 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the attached screenshots. I have a migrated project I need to download to a new installed Windows10 machine. The WinCC version on both PG and Target OS is 7.5. The project is already placed on the path: The name on the server is KALEB5SRV01 and the project is placed on the D-drive on this machine in a folder called WinCC. The name of the project is the same as the name of the server KALEB5SRV01. When I browse my way to the project on the server with the autostart option that is: D:\WinCC\KALEB5SRV01\KALEB5SRV01.mcp After I restart the server it does start WinCC up. When I close WinCC and check the auto path it has been modified to: \\KALEB5SRV01\WinCC_Project_KALEB5SRV01\KALEB5SRV01.mcp I can enter this path as the path of the Target OS in the PG - but every time I click on apply it adds an ekstra directory so the path will be: \\KALEB5SRV01\WinCC_Project_KALEB5SRV01\KALEB5SRV01\KALEB5SRV01.mcp And unfortunately if I do a download it will be a full download and the whole project is downloaded "a level too deep". How do I get the correct path for the Target OS set in the project on my PG? AttachmentP2.zip (124 Downloads) |
Follow us on