4/19/2011 3:52 PM | |
Posts: 8 Rating:
|
See in attachment more information from the device manager on the driver of the cp1616. Best regards, Paul
|
4/19/2011 4:01 PM | |
Posts: 8 Rating:
|
More information about my configuration : System : Intel Pentium Dual CPU E2180 2Ghz w/ 2Go RAM MS Windows XP Pro (version 2002) w/ SP3 CP1616 Softwares : Step7 v5.4 SP5 (cf HSP viewer result in attachment) WinAC RTX 2010 Upgrade Best regards, Paul
AttachmentHSP viewer result.pdf (306 Downloads) |
4/19/2011 6:27 PM | |
Posts: 8 Rating:
|
Hi, (cfC:\Program Files\SIEMENS\SIMATIC.NET\CP1616\inst_bin) I have tested the cp16xxtest.exe with the these params : cp16xxtest.exe trace trace.txt The application seems to have run successfully and you can find the trace in attachment, espescially it allowed me to ensure that the firmware version of the cp1616 was v2.5.1.0. I have found in this document "DK-16xx PN IO PortingInstructions and Layer 2Interface" some example applications to run for testing the driver of the CP1616 (cf driver tests.jpg in attachment). Even if these instructions are destined for testing the porting, i thought it could be used to verify my driver. So i tested the interruption responsiveness and the pnioping and all worked perfectly (cf interruption test and pniopingtest in attachment). So by now i am a bit confused cause I cant figure out why the WinLC is not able to load the cp1616 as a submodule. I don't really know were to look for. Best regards, Paul AttachmentDriver tests.zip (292 Downloads) |
Follow us on