11/15/2021 3:59 AM | |
Joined: 1/17/2013 Last visit: 4/27/2024 Posts: 1081 Rating: (6) |
Dear Experts, I use SIMOTION SCOUT TIA V15 I have 4 servo motor in system but one motor have broken part number 1FK7105-2AF71-1PA0 I would like to replace new motor part number 1FK7105-2AC71-1UG2 but I have stuck at hardware configuration. Have I should to select at Motor with DRIVE-CLiQ interface or Select standard motor from list? IF Select standard motor from list which encoder type I should to select as motor part 1FK7105-2AC71-1UG2 ? Can anybody help me please ? Best Regards, Vorapob AttachmentMotor Change.zip (459 Downloads) |
Best Regards, |
|
11/15/2021 5:52 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, you must select "motor with DRIVE-VLiQ interface and activate the checkbox "Read Out Motor again" |
Follow us on