6/4/2019 2:15 PM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi huzi.saify, There is special library for PID simulation. Or u can write on your own with SCL. The purpose of this is to check HMI IO fields, bar graphs or trends. It has to be removed before applying to actual hardware. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
This contribution was helpful to
1 thankful Users |
6/5/2019 12:57 PM | |
Joined: 4/28/2015 Last visit: 8/7/2025 Posts: 399 Rating:
|
Hello, please have a look here:
Maybe these are the function blocks you are looking for... |
6/5/2019 10:11 PM | |
Joined: 4/23/2015 Last visit: 6/12/2023 Posts: 168 Rating:
|
Personally I don't use a Siemens Library for this, i've just have written my own. This is pretty simple. A very simple way is proposed in this thread https://support.industry.siemens.com/tf/WW/en/posts/software-low-pass-filter-for-s7-1200/81093?page=0&pageSize=10 by Mr. Denilson Pegaia, he proposes a simple basic equation for the first order filter (= low pass filter), you can try this. Pls note that you have to call this equation in a cyclic task, and you will also note that the filter time constant depends on cyclic task callout time. |
This contribution was helpful to
1 thankful Users |
Follow us on