11/3/2010 9:27 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello rolakyng; Writing parameter values to a MM4 drive can be accomplished from the PLC using Profibus, as long as you take a few moments to understand how the Profidrive profile is used. Look at this Application note; it has a few links in section 5, one to a MM4 manual for the Profibus interface, and on to explain how toread/write parameters on a MM4 drive: http://support.automation.siemens.com/WW/view/en/22078757 Start with thois information, and come back when you have more specific questions. |
This contribution was helpful to
1 thankful Users |
Follow us on