3/13/2022 12:22 PM | |
Joined: 8/18/2010 Last visit: 10/31/2023 Posts: 5 Rating: (0) |
Hello Brother, Did you made internal tag named "Shift" into WINCC? Regards, |
3/18/2022 3:45 PM | |
Joined: 8/3/2009 Last visit: 5/3/2024 Posts: 12882 Rating: (1645) |
Hello Salman047 there are a few things to improve: for example if you want to read a Tag then you should use: https://support.industry.siemens.com/cs/de/en/view/109792622/45951188235 -> You miss the Read method and if you want the current Time you have to use "now" instead of "Time" you can also use the ApDiag Windows for Trace outputs. Then you can a kind of "debug" your Script in Runtime. ByeMurof |
Last edited by: Murof at: 03/18/2022 15:45:53If this Information really helps, you could use the Rate function |
|
Follow us on