1/10/2011 6:08 AM | |
Posts: 2964 Rating: (481)
|
Hello Deep, You need to really check after doing the LEC test.... result cannot be judged.... I am attaching you the PDF doc of 802d LEC.... Check it out.... Regards, Ekalavya AttachmentLEC_802d.pdf (339 Downloads) |
This contribution was helpful to2 thankful Users |
1/11/2011 10:56 AM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating: (37) |
Yes Deep , accuracy level will be improved ,check it............. |
Regards, |
|
1/16/2011 8:01 AM | |
Posts: 2964 Rating: (481)
|
Hello Experts, Is the attached procedure same for 840D. If not, can you attached the procedure for 840D, DE, Di. Thanks in advance. DEEP. Hi.... Check out this link /tf/WW/en/Posts/44986#top Regards, Ekalavya |
This contribution was helpful to1 thankful Users |
1/18/2011 11:24 AM | |
Joined: 6/7/2010 Last visit: 2/3/2023 Posts: 569 Rating: (37) |
Hello Experts, Can any one guide me how to connect linear scale to my above system? Thanks in advance. DEEP. Hi Deep, Attached File is the related parameters of linear scale interfacing. you required second encoder feed back controller cardfor it. AttachmentLinear scale.pdf (226 Downloads) |
Regards, |
|
1/18/2011 6:02 PM | |
Posts: 2964 Rating: (481)
|
Hi Deep, If a direct measuring system is connected, the 611UE closed loop control module can onlybe operated with one axis( LT module Single axis). The Profibus address with the appropriate drive number for a single axis power section must be selected
Attachment802D_direct measuring system.pdf (219 Downloads) |
Follow us on