2/17/2012 12:54 PM | |
Joined: 10/3/2010 Last visit: 4/29/2024 Posts: 1552 Rating: (188) |
[quote user="Nikzitronik"]The signed tag has a value of -80 (aquired as you said) and in the IO field I want to multiply it by another tag with a value of 40. Thus the result should be -3200. However I get stars. I have set the lower limit to -10000000 and the upper to +10000000, and the format to s999999. So I guess the limits are not a problem. Note that if the first singed value goes positive, then the IO field displays the multiplication appropriately. Check this: In the Dynamic Dialog, enter as Expression/Formula for example 'SignedTag' * 2 On the right, under Data Type make sure to choose Direct! Could it be that you have 'Analog' selected? |
B r g d s , |
|
Follow us on