10/3/2013 8:21 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
Hi everybody I would like to know if someone know if is possible to work with library "conio.h". and if is possible witch is the procedure. All I found is that http://support.automation.siemens.com/WW/view/es/26731224 The task is that I have to migrate from intouch to WinCC, so the project with Intouch have a lot of scritp with Key. I was wondering if I can build my own function in C, but ANSI C don´t have any function for that. Thanks |
Last edited by: CS Moderator at: 10/8/2013 9:49 AMSubject modified If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
10/4/2013 11:02 AM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
Thanks Yolov for your answer. Well, there is a few functions with that library, but I´m interesting in getch this function prompts the user to press a character and that character is not printed on screen. There isn´t any function included in WinCC C-script for that task, as how not is possible for example works with scanf from stdio.h included in WinCC C-scripts. Thanks |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
10/4/2013 3:05 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
Thanks again Yolov That is what I did . After that I build my own function with VBScrit, and don´t work like intouch, but is OK!. By the way the problem was that Intouch has two keys, for example A1 and go to ..., with WinCC not is possible , but I made a function and now works property. From Intouch ... what I like most is the ArchestrA graphics more than WinCC, with WFC you can build your own symbol, graphics but is more dificult Thanks you very much!!! |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
10/4/2013 3:39 PM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (83) |
You are right!!! Each one has its advantages and disadvantages. Best Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
Follow us on