8/8/2022 9:22 AM | |
Joined: 7/13/2022 Last visit: 2/28/2023 Posts: 17 Rating: (0) |
Hello everyone, I've made an agenda system in LSC and LWE (files in attachment). The idea is to activate an output Q1 on a scheduled basis: the desired days of the week can be toggled on the web page and the on- and off time for each toggled day can be entered in the two fields below it. The time is entered on a 24h basis as a 4-digit value. For example: 9:15am is to be entered as 0915 and 2:30pm is 1430. When I enter these numbers, they are then displayed with the '16#' prefix in their entry fields. Otherwise the system just works and gets activated on the entered time of day. I just want it to be displayed as the number I entered without this prefix. Is there a way to fix this? AttachmentProject.zip (284 Downloads) |
Last edited by: MrPolska at: 08/08/2022 09:23:22Last edited by: MrPolska at: 08/08/2022 09:24:37 |
|
8/8/2022 9:49 AM | |
Joined: 10/16/2020 Last visit: 4/16/2024 Posts: 122 Rating: (12) |
Hi, The next video explains how to fix it. https://www.youtube.com/watch?v=omEMUAlSMJc BR. Cookie_M0nster |
Last edited by: Jen_Moderator at: 08/08/2022 14:01:39Video embedded. If this information has been helpful to you, please don't forget to rate it. |
|
This contribution was helpful to1 thankful Users |
8/8/2022 1:48 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32887 Rating: (4066)
|
This video helps only by old web editors V1.0.x. By using web editors V1.1.x is the new function "Scale time" with the selection "Weekly ON/OFF time". |
8/8/2022 4:45 PM | |
Joined: 10/16/2020 Last visit: 4/16/2024 Posts: 122 Rating: (12) |
Thanks for the clarification. |
If this information has been helpful to you, please don't forget to rate it. |
|
Follow us on