5/15/2008 6:14 AM | |
Posts: 2661 Rating: (279) |
Are you using VMWare? |
5/15/2008 1:28 PM | |
Posts: 10 Rating: (0) |
No, I don't use this... |
Last edited by: recruta42 at: 5/15/2008 3:13 PM |
|
5/19/2008 2:09 PM | |
Posts: 1776 Rating: (95)
|
Hi, do you load the project locally or via network? try to create a new project locally, close and open the project. Does it take also the same long time? |
5/19/2008 4:15 PM | |
Posts: 10 Rating: (0) |
Hi, it loads the project localy.It would be good If I could at least fully open WinCC explorer before the project start loading in the middle of the process. |
5/29/2008 7:52 PM | |
Posts: 10 Rating: (0) |
Well...I am not sure yes..but I am starting to believe it has to do with the size of the Database that was aournt 1.8GB ! |
Follow us on