7/16/2013 1:18 PM | |
Joined: 3/17/2013 Last visit: 6/7/2024 Posts: 481 Rating: (43) |
Hi Experts Does SIMATIC FILED PG-M2 comes under intrinsically safe devices Regards, Vijay |
7/16/2013 1:25 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Please clarify in details what does it mean? Thank you! Best regards, Hristo Mihalev
|
7/16/2013 7:58 PM | |
Posts: 8946 Rating: (999) |
No! |
This contribution was helpful to1 thankful Users |
7/17/2013 10:06 AM | |
Joined: 7/2/2008 Last visit: 5/29/2024 Posts: 928 Rating: (306) |
DearN. Vijay, It is possible to find a PLC in classified area but normally it will be in a classified panel. Classified panels are classified when they are closed not when they are open and for sure you should open them to handle your PLC. I mean there are other things to take care of even when you have what so called intrinsically safe laptops. In a good design for oil and gas and petrochemical industries, all PLCs,RTUs, Remote IOs and even field instruments should be accessed remotely from a decent control room. Anyhow, you can use that thing if you really need it. It's just a sample of how it will look like and for sure you can find more in the market. Best regards. H-H
|
This contribution was helpful to3 thankful Users |
Follow us on