2/12/2024 11:27 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi aamirawan91, In this case, it would have to be the same IP since the Ethernet port that is configured on the PC Station, where the RT Advanced is inserted, is that of the network adapter, so it would have to have the same addresses. I hope this clarification can help you. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on