2/22/2021 9:57 AM | |
Joined: 2/20/2018 Last visit: 5/27/2024 Posts: 46 Rating: (0) |
[snip] I have next question of addressing PUT/GET blocks. Is it possible to use optimized (new standard) blocks for exchange the data between two PLC via S7 connection? (in the manual is suggestion for change to non-optimized, but is it a necessary?). On the SD_1 input in the PUT block I can choose symbolic addressing of some data (despite the fact that according to datasheet should be variant pointer), so why I can not do it the same in the ADDR_1? ------------------------------------------------------------------------------------------ |
Last edited by: Basketballer at: 02/22/2021 10:11:46Last edited by: Jen_Moderator at: 02/22/2021 11:41:43New subject after splitting. Division of question into separate topics. Adam |
|
This contribution was helpful to1 thankful Users |
Follow us on